Hi all,
I have some problems in the IDE of Code Composser. Since 2-3 updates I can't debug one of my boards.
I wil explain a little bit. I have a Kit with 2 boards joined together with some tri-states (MAX3378E) to protect the microcontrollers and maybe the errors I could make. I try to programa with the FET-Pro430 and I could program but with some errors. The problem it is when I enter in the debug mode in the CCS, it says that:
Error connecting to the target:
Unknown device
Some updates (2 or 3) before It works perfectly with the same configuration.Anyone know what happens and how to solve or any idea?
Additionally, I try to separate the boards and i have the same error. I want to add that i could debug the other board without problems, so that means that the MSP-FET430UIF works OK. Could be something relating the tri-state ??
Please help me, I really need to test quikly...