This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPs that support LCD_C Driver.



Hi, MSP Team,

I am looking for a device that meets the following required features.

1. Flash up to 90KB

2. LCD_C driver

3. DAC 12bit 2ch

4. ADC up to 12bit resolution

5. Internal Amplifier

I found the MSP430FG662x and FG642x, but these support LCD_B driver.

It is difficult to find MCUs that support LCD_C driver on the TI.com

Please recommend MSPs that satisfies the above specifications.

  • Hello Sy,

    The LCD_C peripheral is featured on our metering focused MSP430s. So devices that start with part number: MSP430F67xxx. Unfortunately, no DAC module is available on these parts. 

    LCD_C is also featured on our USS metering parts as well (MSP430FR60xx), but they also do not have a DAC module. 

    You can do a TIMER Based DAC with external filter, but you may not get 12-bits of resolution at significant speed. 

**Attention** This is a public forum