Dear all,
I’m working with the GraCE tool.
If the digital IO module is enabled and configured, the GPIO_init.c file is generated with the configuration code as defined in the GraCE GUI. After that, if the IO module is disabled, the file isn’t automatically removed from the file system. I think this situation happens because if you enable it again, makes sense to restore the previous configuration. Unfortunately, when the IO module is re-enabled the information from the GPIO_init.c is lost.
Best Regards,
AES