Part Number: MSP430G2553
Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"I am using the MSP430G2553 chip. I uploaded the code in the chip using the msp430 launchpad board. I want to use the chip in my circuit for ADC and wireless transmission. But when I used only the chip, the msp430 did not work. why? What pins should be connected to get proper output?

"This is the connection made using the msp430 launchpad. But I want to use only the msp430 in my circuit. In the launchpad all the clock, input connections would be connected. But when I take the ic separately, the ic does not work even though the connections were made as shown in the picture. Please tell me what other circuit connections within msp430 should be made with msp430 ic so that the circuit works."
Please help to advise. Thank you for extending your support.
Kind regards,
Marvin