Hi,
I was flashing a change to an example project with my MSP430FR2355 launchpad when I noticed an error in my program. I hit the cancel button and then noticed the configuring debugger executing startup script dialog said cannot be cancelled (see attached 1.png). The dialog then went away. Since this I have not been able to flash the board and get a load program error any time I try to flash the device (see attached 2.png). I deleted the project and reimported the example project however I still get this error. What can I do to reset either programmer on the launch pad or the msp430 itself?
Thanks,
Connor