This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5041: How to write other than specific section in CCS

Part Number: MSP430FR5041
Other Parts Discussed in Thread: UNIFLASH, MSP-FLASHER

Hi,

We are considering the following behavior when debugging is started with a section divided by editing the cmd file with CCS.

[Erase other sections excluding that section → Load a new program into the erased section → Debug]

Is the above feasible with CCS?

We plan to put the user parameter in the divided section, and it will disappear when debugging is started with the default, and we want to avoid the trouble of writing the parameter.

Also, if you want to write the program using MSP-Flasher, uniflash, etc., is it possible to achieve the above?

Thanks,

Eevee

**Attention** This is a public forum