Part Number: EVM430-FR6043
Other Parts Discussed in Thread: MSP430FR6043, OPA836
I have both USS demo boards and want to do water measuring. with the external transducer and FR6047, all work fine, both with standard USS GUI and my own code communicating on the serial interface. When I switch to the FR6043 and use the very same transducer and GUI firmware, I can start the GUI but I can't set the frequency to 1000 kHz even when using the water mode. It ends at 550 Khz - see attached. Any chance to get this to the 1000 kHz for the transducers I m using for water ?
I like to use the external amplifier and hence I connect the transducers to X1 and X2 on the board without changing any of the default jumpers. The code answers with error 0x7e (no transducer found). So what is wrong? Does the external amplifier not support 1000 khz transducers ??