Other Parts Discussed in Thread: MSP430F5529
Hi, on an MSP-EXP430F5529LP board, compiling using gcc, I'm setting up interrupt routines for both TIMER B and USCI A. I'm using code like:
// USCI A1
__attribute__ ((interrupt(USCI_A1_VECTOR)))
void USCI_A1_ISR (void)
{
code
}
// TIMER B CC
__attribute__ ((interrupt(TIMER0_B0_VECTOR)))
void TIMER0_B0_ISR (void)
{
code
}
Now when compiled, the code has:
Disassembly of section __interrupt_vector_60:
0000fff6 <__interrupt_vector_60>:
fff6: 08 47 interrupt service routine at 0x4708
So its got an interrupt for Timer B, but it doesn't create one for USCI A. I can see both are defined in msp430f5529.h
#define USCI_A1_VECTOR (47) /* 0xFFDC USCI A1 Receive/Transmit */ #define TIMER0_B0_VECTOR (60) /* 0xFFF6 Timer0_B7 CC0 */
So what am I doing wrong, its as though the USCI interrupt code is just left out - e.g. it hasn't picked up that its and interrupt routine.