Other Parts Discussed in Thread: LM3S2616
Hi everybody,
I will have to select a Microcontroller for a 1W DC brushed motor with encoder. PWM frequency of about 20kHz. The unit has to be low power. I usually used Piccolo F28027 in most of Actuator designs (motor, piezo-transducer...), but this unit his not really low power.
The idea is to check the features of the MSP430 Family. What's your recommandation of MSP430 model for such an application ?
Piccolos have an integrated eCAP module, which can be used to interface the encode quadrature signals. Is there MSP430 models with integrated module.
Thanks for your inputs, have a nice day !