Part Number: MSP430FR2153
Hi,
I could see that pin P1.1 supports both ADC input and analog comparator input as well. I want to use the same input pin for ADC and eCOMP module simultaneously. The input should go to both modules simultaneously. From the sample code of ADC and comparator module configuration I could see that the register that configures this input pin PxSEL1 & PxSEL0 have same values for ADC & COMP.
So is there any way we could provide this input to both modules simultaneously ?
Regards,
Sai