This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430-IEC60730-SW-PACKAGE: Hardware features required

Part Number: MSP430-IEC60730-SW-PACKAGE

Hi,

We are designing a system which requires IEC60730 certification.

The question is whether IEC60730 certification can be achieved by just using the IEC60730 SW packages or are there any hardware features required to be present in the MSP IC 

**Attention** This is a public forum