This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6970: FRAM write

Part Number: MSP430FR6970
Other Parts Discussed in Thread: MSP-FET, UNIFLASH

Hi,

I want to program 6 bytes of data in FRAM without altering source code, for that i need scripting details using python.

while programming, 6 bytes of data are included with file name, that 6 bytes of data in file name should be written in hex in respective FRAM location.

Example:

file name: MSP430FR6970_44B7D0239811.hex

while programming ,

FRAM[ 0 ] = 44

FRAM[ 0 ] = B7

FRAM[ 0 ] = D0

FRAM[ 0 ] = 23

FRAM[ 0 ] = 98

FRAM[ 0 ] = 11

As above, FRAM should be loded.

**Attention** This is a public forum