Part Number: MSP430F5502
Hi Team,
I'm developing USB device using MSP430F5502. I use MSP430F5502 with ADUM4160(analog device).
The problem is that MSP430F5502 is not enumerate with ADUM4160. (I'm checking on both IC). I had no problem when I checked the usb connection only with the MSP430.
I think the problem is the enumerating timing of adum4160. When I debug my code, the USB interrupt always goes into suspend state.
The question is below:
About enumerate timing of MSP430F5502, is it okay if the d+ line of the msp430 is always pull-up?Is it okay to use 3.3V pull-up at D+ line? Attaching my schematic image below:

Kind Regards,
Jejomar