This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Continuity Tester



Want to design a continuity  tester with below features:

Resistance measurement function with 3 ranges (10 Ω, 100 Ω and 1 kΩ) -

Sound Beeper which makes a sound by a continuity ≤ 10 Ω -

Voltage tester for AC and DC voltage up to 600 Volt -

A flashlight on the rear side -

4 mm female sockets on the top side for measurement cables -

1 button to turn ON/OFF the device -

1 button to turn ON/OFF the flashlight -

Power supply by batteries (e.g. 1,5V AA batteries) -

Protection against accidental connection of a voltage / current source up to 1000V

Can some one from TI suggest with what MCU I should go and how I can get design support in India-Delhi NCR

**Attention** This is a public forum