MSP430FR5729发现有内部时钟,外部接了12M的晶振,发现没有起振,需要如何配置吗?内部时钟可以满足I2C使用吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi jianxiang
内部时钟可以满足I2C使用吗?
Can the internal clock be fully used by I2C?
内部时钟DCO可以满足I2C的使用。精度是全温度±3.5%
The internal clock DCO can be used on I2C communication. the accuracy is ±3.5% at –40°C to 85°C temperature range
Thanks!
内部时钟典型频率是8MHz, 请参考5.16 DCO Frequencies of MSP430FR572x Mixed-Signal Microcontrollers datasheet (Rev. C)
内部时钟需要配置,可以参考3.4.2 CSCTL1 Register of MSP430FR57xx Family User's Guide (Rev. D)
软件配置方法可以参考MSP430FR57xx_CS_01.c of MSP430FR573x, MSP430FR572x C Code Examples (IAR and CCS) (Rev. J)
多谢!
**Attention** This is a public forum