Hi,
I was unable to find this anywhere here on the forums, or in literature here or elsewhere. I need to know if the frequency range specified on the datasheet includes any aging or radiation? Would the MODOSC on the space-hard MSP430 stay within the the specified 3.75 MHz to 5.5 MHz over TID/neutron as well as temperature and with life testing?
Thanks,
Charles