Part Number: MSP-EXP430F5529LP
Other Parts Discussed in Thread: UNIFLASH, TDC7200EVM, , MSP430FR2476
Hi,
I am trying to use the TDC720xEVM Firmware Source provided when installing the GUI for the TDC7201EVM. I can get the microcontroller to interact and take measurements in the GUI, however, whenever I try to use one of the example codes provided in those files, I end up with the error "MSP430:Error initiliazing emulator: No USB FET was found" in uniflash which cannot automatically detect the device. A similar error is also encountered in CCS.
Would you be able to suggest how I could go about having the microcontroller visible to the software? In device manager, it is seen as the TDC7200EVM, there are no other ports such as the MSP Debug Interface.
Cheers,
Paul