This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F67791A: MSP430F67791A SD24INPUT CURRENT

Part Number: MSP430F67791A

Hello.
I have connected SDxN0 and added voltage divided by R19 and R20 as shown in the attached circuit.
When I turn on the power supply, 12mA flows to SD_N, which causes a voltage drop.
I have 6 ports of SDxN0 connected and I think the current value is too high.
Or is it normal?
What would be the normal current value?
Thank you in advance.

AVCC=3.3V
VCC=3.3V
SD_N, SG_1, SG_2, SG_3, AD_REF,TP Measured voltage(0~3.3V) respectively
VASYS1 and VASYS2: Connection
VDSYS1 and VDSYS2: connection
AUXVCC1, AUXVCC2, AUXVCC3 = 3.3V
MCLK 16MHz

**Attention** This is a public forum