Is there a tool out there to program the MSP430F2618 via the BSL? Or does the BSLDEMO get the job done for the f2618 device?
Anyone have any suggestions???
Matt
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a tool out there to program the MSP430F2618 via the BSL? Or does the BSLDEMO get the job done for the f2618 device?
Anyone have any suggestions???
Matt
slau319a.pdf and slau319a.zip have may be useful. Note that for F2xx, the BSL is "ROM Based". The BSL programs on the PC side to handle "ROM Based" chips is inside the "deprecated" folder.
I am using tinyOS-tools to flash 2618.
And that is a script which can be used under linux environment.
**Attention** This is a public forum