Part Number: MSP430I2041
Other Parts Discussed in Thread: ADS1220, , ADS1299
Hi,
Input common mode :
o In the datasheet §8.7.7.4 : Common mode input voltage range [AVSS-1 ; Vcc] : I'm surprised that this doesn't depend on the PGA gain (like the ADS1220), is it really independent ?
o In datasheet §8.7.7.6: "SD24GAINx = 1, Common-mode input signal:?? VID = 928 mV, fIN = 50 Hz":
-> What is the value of the common-mode voltage that gives the values of this field?
-> Do you have a curve of the CMRR as a function of the frequency of the common-mode voltage? (I'm particularly interested in the case where the PGA is 1 [V/V]).
On input impedance:
-> do you have more information? In particular, how do you distinguish part/part variability @ 25°C from thermal sensitivity?
Regards,
Geoffrey