Part Number: MSP430F5659
I have an application for the MSP430F5659 that does not seem to invoke BSL mode on most of the boards I have tested. I have followed the BSL entry sequence shown in figure 1-2 of section 1.3.1.1 of the SLAU319AF. One board enumerates itself to our host system as a USB HID device which is good. Two other boards tested come up in our application mode and do not invoke BSL mode under the same conditions. I found an errata, USB11 published in the SLAZ493AA, that indicates seems to indicate that external entry into BSL mode basically does not work. Please provide any more information available on this issue.