This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: MSP430FR6043 ADC Sample time guidance

Part Number: MSP430FR6043


Hello Community,

In the datasheet, I read the 8.13.10.2 12-Bit ADC, Timing Parameters. The minimum and maximum frequency ranges of that fadc are 0.45 Mhz and 5.4 Mhz, respectively. Then I shouldn't cross the Fadc max (5.4 Mhz), am I correct? 

The ADC clock should be less than 5.4 Mhz..?

How to find the tsample time ? Is there any formula to calculate the tsample?

In datasheet, min tsample time mentioned as 1 μs and what about tsample max?

Consider I want to sample at 1ms and my Fadc clock is MODOSC (5Mhz). what value I have to select for ADC12SHT bit.

Thanks in advance,

Sarwath

**Attention** This is a public forum