Hi Team,
There's an issue from the customer need your help:
In the document linked below, it is stated that the frequency sweep is determined by 50% of the peak amplitude to determine the F1 and F2 frequencies. It can be seen from the image that the peak amplitude is about 1100, so why the final selected F1 and F2 frequency point peaks are More than 600, the other is 300. Not 50% as described.
Thanks & Regards,
Ben