Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP-FET
Hello,
I am trying to validate Timer2_A2 settings via EEM and Clock Control features, available through the MSP-FET debugger.
EEM Version S should provide Extended Clock Control on Modules. So I enabled it in the debugger session for all Timers.
When debugging the following instructions (with a breakpoint just after the third instruction and the code running in FRAM with NWAITS = 0),
mov.w #TASSEL__ACLK|MC__CONTINOUS|ID__1|TACLR,&TA2CTL nop mov &TA2R,R12
with:
DCO frequency = 8MHz
MCLK = 4MHz
ACLK = 32kHz
I find largely different values between R12 and TA2R (shown in the Timer2_A2 group window), slightly varying every time I repeat the same test. For example:
- test 1: R12 = 0x0056C, TA2R = 0x3455
- test 2: R12 = 0x00547, TA2R = 0x360A
- test 3: R12 = 0x00581, TA2R = 0x33FD
Every other interrupt is disabled. So my questions are:
a. Why R12 and TA2R values differ so much?
b. A 'nop' instruction executes in only 3 MCLK cycles, so why TA2R (triggered by the much slower ACLK) is not zero after a single 'nop'?
Thanks in advance for any clarification.
Regards,
Mauro