This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR59941: Internal Flash Memory - Write & Read

Part Number: MSP430FR59941


Hi,

I need to write and read 2 bytes of data from the internal memory of the microcontroller.

If the power is off, the two bytes do not get erased.

How can I write to and read from internal memory?

Is there an example code available?

Thanks & Regards,

Vijay

**Attention** This is a public forum