Part Number: EVM430-FR6043
Hello,
I am using EVM430-FR6043 and Ultrasonic Sensing Design Center GUI to design a gas flow meter. When I select EVM430-FR6043 Gas as the meter option, VFR Flow + Temperature Calibration is disabled (Every part in the VFR Flow + Temperature Calibration tab is greyed out). Is there a way to use this feature for the EVM430-FR6043 Gas meter? Why is this calibration mode blocked in this mode? Is there a specific reason why this section is disabled for the EVM430-FR6043 gas meter?
I was looking through the TI USS library and the template code and found a few functions such as USS_calculateVolumeFlowRate, USS_initialSearchQuad, and USS_calibrateVFRFlowTemperature which I am assuming are used in VFR Flow + Temperature Calibration feature. I would like to know if the FR6043_USSSWLib_template_example code is the same as the one already loaded on EVM430-FR6043 and whether I could gain access to the VFR Flow + Temperature Calibration feature if I design my code utilizing these functions. Since EVM430-FR6043 successfully connected to the Ultrasonic Sensing Design Center and is functioning, I assumed that the board came with the default code loaded onto it. Is this the same code/program as FR6043_USSSWLib_template_example? Will the board and the GUI work the same as now even when I load FR6043_USSSWLib_template_example code again to EVM430-FR6043 using CCS?
Thanks in advance.