Part Number: MSP430F2131
Hi team,
The Brown Out Reset occurs when the voltage falls below V_HYS (B_IT-), which is at most 1.92 V [1, page 20].
If we want to operate the microcontroller at 12 MHz, a minimum of 2.7 V is required [1, page 14].
What happens if the supply voltage drops below 2.7 V, but not below 1.92 V, so that the Brown Out Reset is not triggered and the supply voltage is insufficient?
BR,
Stefan