This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SEH Sensor Monitor Error



Hi, I have imported the SEH Sensor Monitor from the development kit and can't get the thing to debug. I am getting the error C:\Texas Instruments\eZ430-RF2500-SEH_Sensor_Monitor-v1.3\CCE_Source\Projects\Examples\peer_applications\eZ430RF\SEH Sensor Monitor\End Device -Debug\APasdatahub.out not found which is canceling the launch because the program file does not exist. I am very frustrated and have been trying to iron out this issue for several days and any help would be very much appreciated.

 

Thanks,

 

Alex Revello

  • Citing which software you are actually using proved to be helpful.  Thank you for including that.  It was not clear in your other posts on the following thread.

    When I downloaded the eZ430-RF2500-SEH software, it was version 1.5, not version 1.3.  However, I suspect there is enough similarity to help you get through this problem you face.

    You state you have an error that the APasdatahub.out is not found.  Are there any other errors that were reported in the build process that might clue us into why the APasdatahub.out was not found, such as :

    error: unresolved symbols remain

    error: errors encountered during linking; "APasdatahub.out" not built

    If you do receive this, have you setup the DEV_ROOT path variable that is discussed in the README.txt file in the <EZ430_RF2500_SEH_INSTALL_DIR>\CCE_Source directory?

    If you have not done this, go to Window->Preferences... in the CCS menu.  Navigate to General->Workspace->Linked Resources.
    Add DEV_ROOT and set to the location where you installed this software up to the following sub-directory :
    <EZ430_RF2500_SEH_INSTALL_DIR>\CCE_Source

    Then try to rebuild.

  • Thanks so much now I can start working :)

**Attention** This is a public forum