Other Parts Discussed in Thread: SYSCONFIG
Hi,
I'm using LP-MSPM0G3507 board. I have debugger connection issue when I'm trying to flash the board from CCS :
"CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset. If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information."
It was ok until I selected pin PA18 as an UART pin. After I flashed it ones with the UART pin it started all those connection issues.
As I see on datasheet, PA18 is also BSL Invoke pin. I tried to make a Factory Reset for the memory but it still unable to connect the board for the reset.
It seems like the NONMAIN MEMORY has been corrupted.
How can I reset the chip to its factory settings? The help will be appreciated very much!