I have a MSP430F5529 on the board. Following are the hardware design for the clock.
1. One 12MHz crystal connected XIN and XOUT, each terminal with 22pF caps
2. One 32.768KHz crystal connected to XT2IN and XT2OUT, each terminal with 22pF caps
Everything works fine, but the clock (MLCK) is running at the low frequency. I looked at the output of MCLK, it runs at about 1.4MHz. How do I make it run at higher frequency?
I have tried different clock settings for the registers of UCS, but could not get it work faster.
Thanks and regards
Wen