This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: HID Bridge Firmware Flashing

Part Number: EVM430-FR6043
Other Parts Discussed in Thread: MSP430F5528, UNIFLASH, MSP-FET, MSPDS

Hello,

I am designing using EVM430_FR6043 but would like to move on to the custom board using MSP430-FR6043. Since I will be using the Ultrasonic Sensing Design Center GUI for debugging purposes, I plan to integrate M430F5528 (HID bridge) as well.

On the forum, I read about HID Bridge Communication Firmware (MSP430F5528) and downloaded the file that was provided on the post (/cfs-file/__key/communityserver-discussions-components-files/166/TI_5F00_MSP_5F00_HIDBRIDGE_5F00_eZFET_5F00_USS_2D00_EVM.zip). Does this contain the most recently updated version of the firmware for HID Bridge (The current version is: TI_MSP_HIDBRIDGE__1_00_03_00__BANSHEE-USS-EVM.txt.)? The instruction says to use MSPFlasher and execute Program_AIO.bat to automatically flash both the EZFET file and HID_Bridge file to the respective MCU. Is it possible to flash the HID_Bridge file through a USB_serial connection using UniFlash or MSP430 USB Developer Package? Or is it necessary to have EZFET integrated into the custom board? What if I use MSP-FET instead of EZFET?

Thanks,

Min

**Attention** This is a public forum