This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello! For my application, I'm trying to jump back to the address stored in the reset vector 0xFFFE. I'm using `asm(" BRANCH &0xFFFE")` to do so. This seems to work alright in normal operation, but if I pause execution before the instruction and try to step through (like I was when trying to verify it works), the PC is always loaded with 20 bits from the memory at _reset_vector instead of 16. This is the case even if I skip the emulation instruction and use `MOV.W` directly. For example, with the memory below, I would expect the PC to be loaded with 0x06EAE, but it is loaded with 0xF6EAE instead. This only occurs when I pause execution at or just before the branch instruction. If I am simply connected to the debugger and start running from main, there is no issue. This is not the first time I have been burned by this behavior; am I missing something here? Why would a branch instruction load a 20-bit PC even with small code model?
Hi Jacob,
The volatile keyword fixing this points to potentially the compiler being the source of the issue. Which compiler/IDE are you using?
If CCS, can you go to View -> Dissassembly while debugging, and see what the actual assembly instructions look like in both cases?
Best Regards,
Brandon Fisher
I don't see a "BRANCH" mnemonic. Just "BR" and "BRA". The first always clears the upper 4 bits while "BRA" is the extended version.
Section 6.6.2.8 of the MSP430x5xx user guide is titled "BR, BRANCH", and for other opcodes that is the mnemonic. I took this to mean that either "BR" or "BRANCH" will "Branch to destination in lower 64k address space". I believe I tried all three of "BR" "BRA" and "BRANCH" and had the same results.
I'm using CCS. When debugging with no volatile, It shows `BR &_reset_vector` with opcodes `0x0200 0xFFFE`. With volatile it is the same mnemonic but opcodes `0x4210 0xFFFE`
Opcodes beginning with a zero like 0x0200 are a MOVA instruction and thus 20 bits. Those starting with a four are MOV.
Why the use of volatile is changing things I don't know. With the GNU compiler it disables some optimizations that could cause trouble. Or so says the docs.
I tried this with GCC and checked the output. BRANCH it didn't like, BR generated a MOV, and BRA a MOVA. All without a volatile tag.
It looks to me then this is just a nuance related to how the compiler is optimizing this code. I will see if our tools team can comment.
I don't necessarily expect the compiler to be optimizing inline assembly statements (unless it determines they are unreachable), but my expectation may be incorrect here.
Best Regards,
Brandon Fisher
For the source file with the problem asm statement, please follow the directions in the article How to Submit a Compiler Test Case. After you have created the preprocessed file, add a comment that shows the asm statement in the form where it works, i.e. with volatile.
Thanks and regards,
-George
**Attention** This is a public forum