This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6769A: I want to update the microcontroller on my device via wireless communication.

Part Number: MSP430F6769A
Other Parts Discussed in Thread: CC1310

Hell,

Please tell me if it is possible.

First of all, I would like to know if 1 is possible, and if so, I would like an idea for 2.

For example, let's say you use MSP430 on the board.

Connect the wireless transceiver to the MSP430 for serial communication.

At that time, I would like to retrieve the update data from the PC, disassemble the device, and use wireless communication without having to connect via JTAG.

What I want to ask is,

1:Can I connect a wireless transceiver to MSP430?

2:If I can connect a wireless communication transceiver to the device, can I use the wireless controller to send update data from the PC to the device?

Is it best to design a board that has a USB connector and a wireless controller?

First of all, I would like to know if 1 is possible, and if so, I would like an idea for 2.

thank,

**Attention** This is a public forum