Hi,
MSP430F6436 freezes at low frequency during power-up. When viewed in debug mode, the debugger also seems to give a message that points to an address that deviates from the programme and is probably out of control. It is operated using an external 32.768 kHz oscillator. 1 MHz main clock is generated from the 32 kHz oscillator, with the DVCC running at 3 VDC and the PMM at default. Looking at the amplitude of the oscillator, it produces about 32 kHz but only about 0.2 Vpp amplitude, so it is questionable whether it is really working correctly. Is this amplitude OK for the msp430? If there is a problem, can it be corrected on the software side? Or is it necessary to take measures on the hardware side?
msp430 external oscillator.xlsx
The following crystals are used.
SCX Series (SC-32S) SMD Type Quartz Crystal
https://www.sii.co.jp/en/quartz/datasheets/smd/sc-32s/
Thanks,
Conor