Part Number: MSP430FR2355
CCS is throwing an error with a damn for loop iterator for no reason.
volatile unsigned short m = 40, M = 72; volatile unsigned int P;
for (int i = 1; i <= M; i++) {
P += m;
}
When I compile, the for loop line throws errors 29 "expected an expression" and 20 "identifier 'i' is undefined" even though I'm f**king defining it right there. Changing data types doesn't help, neither did setting int i=0 and making the comparator 1<M. I had to predefine i above the for loop to clear the errors.