Other Parts Discussed in Thread: MSP-FET, MSP430F6769A, MSP430F4783
Hi,
I would like to receive ideas.
I want to update the firmware of MSP430 using USB.
The MSP430 is inside the machine, but with J-TAG, the machine would have to be dismantled, so I would like to update it so that it cannot be opened.
Therefore, since the machine has a USB interface, I would like to import data from there.
I thought that if I use MSPBSL, I can bridge the PC and USB.
However, the PC side can be connected via USB, but the 10-pin side cannot be connected to MSP430 unless it is converted to USB.
In the first place, like MSP-FET, is this also used on the premise of J-TAG?
If so, I would like to know how to update via USB instead of via J-TAG. Please let me know if you have any ideas.
Thanks,