This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Device Selection Inquiry (MSP-TS430PM64A)

Other Parts Discussed in Thread: MSP430F4152, MSP430F2234, MSP430F2370, MSP430F2350, MSP430F2330, MSP430F2274, MSP430F2254

Hi,

 

We have a kit contents called MSP-FET430U64A which contained one MSP-TS430PM64 target socket module with two unit of MSP430F4152IPM. We would like to run an application that flashes the LED, step by step procedures were followed as shown in user’s guide. But somehow we are facing problem in communicate the MSP-FET430U64A  module to MSP430 USB-Debug-Interface module. From the GUI to select the target device, we are not able to find MSP430F4152 device. Any idea why it can happen?

Appreciate your prompt reply.

 

  • Which GUI you're using ?

    if it is IAR;

     

     

  • Hi,

    Thanks for the reply. I was downlaoded this IAR Embedded Workbench Kickstart software from the website which prompted from installed CD. The software descrption as stated below where the GUI without MSP430F4152 device. Any idea for me to download the GUI as shown in figure above? Appreciate your prompt reply. Thanks

    Product Information

    IAR Embedded Workbench Kickstart for MSP430 is an integrated development environment (IDE) for building and debugging embedded applications for MSP430 microcontrollers. The IDE includes a 4K limited C-Compiler/Unlimited Assembler/FET Debugger/Simulator. The FET Debugger is a fully integrated debugger for source and disassembly level debugging with support for complex code and data breakpoints.

    Tool Name: IAR Embedded Workbench Kickstart Version 3 (Rev. L)

    • Contents: IAR 3.41G/WIN, FET 4.53/WIN
    • Updates: Added support for MSP430F2234, MSP430F2254, MSP430F2274, MSP430F2330, MSP430F2350 and MSP430F2370
      Includes the latest MSP430 device support files and MSP430.DLL driver module.
    • Supported Tools: MSP-FET430PIF, MSP-FET430X110, MSP-FET430P120, MSP-FET430P140, MSP-FET430P410, MSP-FET430P430, MSP-FET430P440, MSP-FET430UIF, MSP-FET430U14, MSP-FET430U28, MSP-FET430U38, MSP-FET430U40, MSP-FET430U48, MSP-FET430U64, MSP-FET430U80, MSP-FET430U100 and EZ430-F2013

     

  • I am using 5.30.1 Kickstart Edition.

    You can download this software this link;

    http://dl-www.ti.com/lit/sw/slac050/slac050.zip

     

    IAR EW Wiki Page

    http://bit.ly/oZfNlo

     

  • Hi M.Fatih,

    Thanks for the information and the link provided. I'm successfully to select my device from this version 5.30.1. Appreciate your helping. 

    best regards

**Attention** This is a public forum