Other Parts Discussed in Thread: EVM430-FR6043
Hello Team,
There are 2 questions that need your help,thanks!
1. Could you pls share the MSP430FR6043 source code, we need to do secondary development on it, for mix gas ultrasonic flow meter;
2. The development board EVM430-FR6043 was connected to the TI PC software USS, it was normal at the beginning, and our own ultrasonic sensor was connected to the development board, the frequency is 1MHz, after modifying the frequency parameters on the USS modification several times, the USS and the development board can not communicate normally, the details are as follows:


The computer development environment.