Part Number: EVM430-FR6047
Dear TI,
I am writing this ticket to equire about other informations regarding the module data exit modes.
I am using your product in combination with a time of ultrasonic time of flight sensor, for a high time-resolution application in a fluidic mock up of aortic vessels.
The first question is: is it "plug and play" with an arduino possibily? (maybe using the RXD - TXD ports or some other kind of port) ?
If so could you point me to any available tutorial/ documentation? (a raspberry or any other kind of unit with a microcontroller would be fine as well.
I have an arduino already implemented for pression sensing, and I would like to combine all units together.
I would like to have the video output in a unit removed from the board itself, is there any way I could buy an identical display to move somewhere else while desoldering the one you have mounted on the board? or maybe if its not for sale you could share with me an identical model or maybe even just the logic it uses for powering and driving the dispay?