Trying to confirm how many oscillators we really need in our project. Diagram shows 3 of them - One 32 kHz and two at 8 MHz.
In section 9.13.2 Oscillator and Clock System (CS) of the MSP430FR6043 Data Sheet it says :
"The high frequency oscillator XT2 (HF) can be sourced from the oscillator of the ultrasonic subsystem USSXT through an internal connection."
What register needs to be set to enable sharing of this clock between the USS module and XT2 ?
Are there any side effects to sharing the oscillator or other things to consider?