This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779A: LCD C charging pump capacitor problem

Part Number: MSP430F6779A

I have question about LCD C charging pump capacitor problem (found from our customer site).

Step 1) With 4.7uF charge pump capacitor Measure the voltage on the capacitor 3.2 v.

Measure the capacitance of the capacitor 5.3 uF.

The LCD module does not have segmented and common signals.

Step 2) After disconnecting and the reconnecting the 4.7 uF charge pump capacitor (same one).

Measure the voltage on the capacitor, 3.5 v. Measure the capacitance of the capacitor, 5.3 uF.

The LCD module has signals to the segments and segments.

Could you please explain to us that something is wrong?

(e.g. the LCD module damage or something)

Note:

configuration we use

LCDCPEN = 1, VLCDx = 1111

**Attention** This is a public forum