Part Number: MSP430FR6043
Other Parts Discussed in Thread: EVM430-FR6043, MSP430F5528
Hello,
i have some question regardings the MCU MSP430FR6043.
1.For the EVM430-FR6043 is it possible to add a Temperatur sensor to calcurate the calibrated flow with temperature? when yes at which pin should i use.
2.Does the MCU have an Digitaloutput and Anlogoutput as well as Digitalinput? when yes is there any way to test them via the The Evaluation board above? ist the analogoutput current, or voltage? what is the resolution for analogoutpunt and Digitaloutput?
best regards.
Pierre Ngirinshuti