This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: get stuck on RF_runCmd()

Part Number: LAUNCHXL-CC1310

Hi Team,

Example: Simplelink_cc13x0_SDK_4_20_02_07

Issue: when running, both CCS and IAR are stuck at RF_runCmd().

Could you help check this case? Thanks.

Best Regards,

Cherry

  • Hi Cherry,

    Can you post some more detail about your issue?

    1) Which example project are you basing your project on?

    2) Which command are you sending when the device is stuck?

    3) Can you pause the program when this happens and post your call stack?

    4) Can you give more context for what you are trying to achieve?

    Cheers,

    Marie

**Attention** This is a public forum