This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: Absolute TOF drops to 0 in high wind. But ADC Captured waveform seems OK

Part Number: EVM430-FR6043


Hi experts,

I'm testing the EVM430-FR6043 in a wind tunnel with 200 kHz transducers. Everything works fine until it reach high wind speeds (around 100 km/h, and above). At this point th Absolute TOF measurements drop to 0 (and also the Delta ToF). But the ADC Capture waverform at this point seems to be OK. I tried different "GUI Based Gain Control dB", to increase or decrease the captured waveform and don't observe any improvement.


Figure 1. Increasing wind speed until 100 km/h. Decreasing wind speed after some time at 100 km/h:

Figure 2. Typical ADC Capture waverform al 100 km/h. Different "GUI Based Gain Control dB" modify the amplitud, but the Absolute TOF measurements remains at 0.

 

Figure 3. Basic configuration of the EVM.

Figure 4. Advanced parameters of the EVM.

What could be causing the measurements to drop to 0? Recommendations to improved that?

Best regards,

**Attention** This is a public forum