This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6047: MSP430F5528

Part Number: EVM430-FR6047
Other Parts Discussed in Thread: MSP430F5528, EVM430-FR6043

Hello, 
I have a queston on EVM430FR6047 and namly on the part MSP430F5528 COM MUNICATIONS HID-BRIDGE. 
I want to change the USB bridge to RS485 bridge. is it possible to directly use it? how should the circuit look like? or do i need  a Bridge to convert into RS485? if yes, is there a TI part i can use? how does in this case, the circuit looks like? 
when i use now RS485 which file in the Software do i use in order to adjust the communication parameter? 

best regards
Pierre Ngirinshuti

**Attention** This is a public forum