This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5234: Linux sample source code regarding the TPS2388x PSE system firmware host interface protocol?

Part Number: MSP430F5234

Dear TI Specialist,

      Could you provide the Linux sample source code regarding the TPS2388x PSE system firmware host interface protocol?

We need it so that the CPU (host) can communicate with the MPS430(FirmPSE) through the I2C bus to get/set the relevant registers.

Example: System PoE Enable 0xE/0xF GET/SET: MCU will wait for this command if system boot up setting is set to wait for host

Regards,

Gary

**Attention** This is a public forum