Part Number: MSP430F5529
Hi Experts,
I was trying to achieve a USB interfaced project using MSP430F5529 using USB descriptor and CDC class
when i try to upload code into the board showing error unknown device like,

the steps i have taken to upload the code is,
- Generated CDC files from USB Descriptor
- Imported C1-LEDOn/Off project
- copy pasted the generated files from USB Descriptor including Inf file
- Build happen
- I kept GND, 5V & 3V3 jumpers and removed remaining(i hope this is the way to do an USB Project)
- connected the USB cable to the host computer
- and clicked run
Ports Shown:
1. UART1
2. Debug Interface
3. USB serial Device
Working with the USB serial device port
Also i connected all jumpers and uploaded the code still LED not blinking (don't how to do it actually but eager to learn about it :-) )
and the error coming as mentioned in the above image
Please help me, any suggestions will be greatly appreciated!
Best regards,
Tex