Part Number: MSP430FR6043
In order to reduce FRAM consumption I'm trying to set a same common trap-handler to multiple interrupt vectors on MSP430FR6043.
With the TI compiler this is possible using "pragma vector":
#pragma vector=RTC_VECTOR, PORT2_VECTOR, …, UNMI_VECTOR
__interrupt void Dummy_ISR(void) { while (1) { } }
Is there an equivalent for MSP430 GCC compiler 9.3.1.11, which uses "__attribute__((interrupt(x)))"?
On MSP430 irq handlers and vectors with gcc there is a hint, but it fills the memory every 32-bit instead every 16-bit (the vector table has 16-bit elements!).
Example msp430fr6043.ld:
MEMORY {
…
UNUSED_VECTS_1 : ORIGIN = 0xFF90, LENGTH = 0x004C /* END=0xFFDB, 38 vectors, size 76 bytes*/
…
}
SECTIONS
{
…
__unused_vectors_1 : { KEEP (*(__unused_vectors_1)) } > UNUSED_VECTS_1 /* 0 - 37 = 38 vectors */
…
}
traps.c:
static void __attribute((interrupt)) default_trap(void) {
while (1) { }
}
__attribute__((section("__unused_vectors_1"), used))
static void (*vectors[19])(void) = { // 1. compile ok, but elements are 32 not 16-bit!
//static const uintptr_t v[19] = { // 2. compile ok, but elements are 32 not 16-bit!
//static const __int20 v[19] = { // 3. compile ok, but elements are 32 not 16-bit!
//static const uint16_t v[38] = { // 4. compile error: initializer element is not computable at load time
default_trap, // unused
default_trap, // unused
default_trap, // unused
default_trap, // unused
0, // intentionally left zero to check the result
0, // same as above
};
In the above traps.c snippet, the first 3 forms compile, but the result is wrong. For example if the resulting address of default_trap is 0x99FA, then the resulting memory content at 0xFF90 is: 99FA 0000, 99FA 0000, 99FA 0000, 99FA 0000, 0000 0000, 0000 0000, .... but what I expect is 99FA, 99FA, 99FA, 99FA, ....
If I try to force the table to be 16-bit (the form 4 in the above traps.c), then the code doesn't compile, failing with the "initializer element is not computable at load time" error!
Any suggestion how to achieve this with GCC using any C/ASM/Linker combination? Thanks!