Other Parts Discussed in Thread: MSP430F5528, MSP430F5529
Hi, I'm looking for some positive confirmation here that my hardware setup will work.
I was reading through SLAA452b and got to section 3.7. The text there reads: "The on-chip BSL needs to know the reference frequency to configure the PLL. By default, it is able to detect the presence of four frequencies on XT2: 4 MHz, 8 MHz, 12 MHz, or 24 MHz. If it finds one of these, it programs the PLL accordingly." In my hardware setup, my only clock is a 8MHz silicon oscillator feeding the XT2 input, but I noticed that all of the TI target boards have crystal oscillators on both XT1 and XT2 inputs. Will the BSL automatically know to set the XT2 to bypass mode to find the 8MHz clock or do I need to use a crystal oscillator?