Other Parts Discussed in Thread: TINA-TI, TIDA-01486
Hi
I have bought the TIDA-01486 booster pcb and connected it to the EVM-FR6047. However I noticed that I had an ok echo over the transducer (1MHz frequency 80mV pk-2-pk, while I could only see a very weak echo when performing the adc capture with the USS design center program. After investigating I noticed some differences between the TINA-TI model provided for the TIDA-01486 and the schematic.
In the simulation model

And the Altium schematic

Besides the different value for C7/C49 (which made the response better for my use), the C53 capacitor here seems to give negative gain when simulating, which also seemed to be in line with what I observed during testing.
However after removing the capacitor, I now seem to have stability problem as I see a lot of oscillations. I just wondered why the 2.2uF was added in the first place? Seems like the booster card cannot achieve 50db gain if I have done the simulation correctly.